Cancel
Showing results for 
Search instead for 
Did you mean: 

experiment manager passing time or real values to output

Creator
Creator

Hi everyone,

 

I am using experiment manager to run my model with several different input parameters. First I fill a whole table based on 1000 entities that have passed through the system. Once 1000 entities have passed through I perform some calculations on the 1000 entities that have passed through, which gives me the following 5 outputs:

 

- average cycle time

- standard deviation of cycle time

- average tardiness

- fraction on time 

- reliability of the lead time

 

These 5 values are all of the data type "time". However, once I run the experiment manager, it says:

"a 'time' cannot accept the method 'copy' " and consequently I am not able to extract the output for the several input parameters. Does anyody have any idea how I can still give these 5 values as output to the experiment manager. 

 

I already tried changing the output values to data type 'real', but then I get the same error.

 

Help is very much appreciated! Smiley Happy

 

Kind regards,

Noud

1 REPLY 1

Re: experiment manager passing time or real values to output

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello Noud,

 

If the model doesn't contain sensitive information, could you upload it to the forum? This makes it easier for us to understand your problem instead of trying to replicate it ourselves.

 

Thank you Smiley Happy

Nick Peeters
Simulation Consultant
www.cardsplmsolutions.com