Cancel
Showing results for 
Search instead for 
Did you mean: 

experiment manager using dialog

Creator
Creator

Hello,

 

I want to fill the insert fields of my experiment manager with values and dropdownlist indices from my dialog.

 

Unfortunately i get error messages that i chose the wrong insert value.

 

Is there a way to fill the experiment manager with data from an dialog by inserting the correct path?

Or is this in general not possible?

 

Thank you very much for your help!

 

Seraphin

 

Unbenannt.PNG2.PNG

1 REPLY 1

Betreff: experiment manager using dialog

Gears Phenom Gears Phenom
Gears Phenom

Hello Seraphin,

this is not possible:

input values must allow an instruction like x := x

The ExperimentManager cannot change the input value in a dialog, because it uses setValue for applying the input value and getValue for reading it. But it also makes not so much sense to do it, anyway, because the input-values are to be changed by the ExperimentManager for different experiments, and what good would it do to change some dialog-elements? If you are using the value of dialog-elements in your model, then save them into variables/tables/attributes from the dialog and use those in the ExperimentManager.

I hope this helps Smiley Happy
Alex

___________________________________________________________
Alex Dilg, Consultant at SimPlan AG (www.SimPlan.de)
This post was good and/or helpful to you? Please provide some Kudos, thank you!