Cancel
Showing results for 
Search instead for 
Did you mean: 

formula for setup times

Builder
Builder

Hi community

 

I have a simple problem with a formula to set the setuptimes from a table. I have created my own arrangement in a table, but I can't set the correct structure of the formula. II'm using this type of table because the setup time is different from machine to machine and the matrix table doesn't work for me. I have attached an image.

 

Thanks in advance, I appreciate your help

 

Regard

Charly

2 REPLIES 2

Betreff: formula for setup times

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Charly1,

 

just modify the last line of your method:

result := SetupTimes[Modelo, Operation]

 

This should work.

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Betreff: formula for setup times

Builder
Builder

Hi GG

 

Thanks for your help...

 

It works perfectly!

 

Regards

Charly