Cancel
Showing results for 
Search instead for 
Did you mean: 

from

Experimenter
Experimenter

 
s

 

 

1 REPLY 1

Re: Mu's from source

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

you can have a look at the attached example model, there something similar to what you have described is implemented in a simplified setting. The MU is producing every 5:00 minutes a MU according to the time interval that is set in its attributes. Then the exit of the source is locked after the last e.g. 23rd MU has left it using its own exit control. Afterwards a generator object unlocks the exit of the source after 8 hours again. You could also use the methods implemented in this example to get such a behavior in your model.

Kind regards,

Igor
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution