Cancel
Showing results for 
Search instead for 
Did you mean: 

have access to next succ on exit

Pioneer
Pioneer

Hello

 

I would like to know how to write in method to know to which next object Plant has to push a Mu.For example I have Mu on line with exit strategy cyclic. I would like to know if the Mu will go to SingleProc or SingleProc1 when this Mu is blocked at the end of the line :

 Capture.JPG

 

thanks for your support

Christelle

5 REPLIES 5

Re: have access to next succ on exit

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi Christelle,

 

In general it is not possible to know beforehand where an MU will go, since this depends on the exit strategy settings AND on which successor becomes available first. The only exception is when Blocking is active. But it kind of makes no real sense, to retrieve this information you would probably use some exit control. If you have an exit control in place, you would use that to set the next successor, not?

 

 If you can share some backgrounds of your question, we may be able to help you a bit more.

 


Gert Nomden
Digital Factory Consultant
cardsplmsolutions.com

Re: have access to next succ on exit

Pioneer
Pioneer

I tried to use several HBW in my frame, my Mus can go to both of them. I tried to use only one WMS but no success then I thought to use 2 WMS and when Mu needs to go toRackLane I have one condition in the userSetTarget and other way other condition :

in my example I tried with destination in MU but Mu don't go in RackLane1.

Do I need to program only by method to have such event :

Capture.JPG

Thanks for your support

Re: have access to next succ on exit

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

As far as I know, you can connect the rack lanes, like in the example model (Examples collection). Then the products should be routed correctly.


Gert Nomden
Digital Factory Consultant
cardsplmsolutions.com

Re: have access to next succ on exit

Pioneer
Pioneer

In the example you sort products (specific rack), in my case one type of product can go to both of rack.

I want to put product by two in one rack then 2 next to second rack (the 4 products can be same type of product)

How do I proceed ?

Thanks for your collaboration

Re: have access to next succ on exit

Phenom
Phenom

Hello

 

If you do not mind the call happening at a slightly different time, you could look into the pull control of the singleProcs, in doing so you can run some code from the singleProc before it gets the MU, and have full control over when the singleProc will take that part in still.

 

Hope this helps you,

JamesM