Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

help to build the general modle

Experimenter
Experimenter

Hello 

i  use Plant simulation since two weeks to build a modle for production line. 

 

i need help in building  the general modle of this production line.

i don't know how can i represent the Raw Material  coming from warehouse 1 (red arrows) to diffrent workstation (XX_WS) using the SOURCE ?

how can i represnet the PP_WS with two machine ?

 

how the GENERAL modle  should look like 

 

Thank you in advance

 

 

1 REPLY

Re: help to build the general modle

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Assuming your warehouse doesn't run out of supplies use 1 source per warehouse.

 

Use a table to produce a sequence or random PP in your Source involving all different parts for each warehouse.

 

Then use the Source tab exit strategy select MU attribute or add a flow control object after each source to direct the parts to the right succesor (machine).

 

In the help look for all this topics so you can understand what you are doing:

  • MU selection
  • Exit Strategy
  • Flow control
  • Successor  
cortega@interlatin.com.mx
+52 (81) 10801310
InterLatin S de RL de CV