Cancel
Showing results for 
Search instead for 
Did you mean: 

how to analyse collision between walking workers?

Experimenter
Experimenter

i want to analyse collision between workers when they walk on the footpath

 

which one to select from the ''class library'' to start analysing collision?

 

thanks in advance

2 REPLIES

Re: how to analyse collision between walking workers?

Siemens Phenom Siemens Phenom
Siemens Phenom

You cannot detect "collisions" of workers. (At least there is no easy way to do it.)

In reality two workers will always find a way to pass each other. So it seems to me that there is just no need to detect such a collision.

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: how to analyse collision between walking workers?

Experimenter
Experimenter

Thank you Michael for the reply

 

 i would like to simulate the collision between 2 workers when each is carrying a box.

 

the footpath is narrow for 2 workers carrying boxes to pass each other comfortably thus the need for the collision analysis. 

 

is it possible to simulate the collision when both are carrying boxes?