Cancel
Showing results for 
Search instead for 
Did you mean: 

how to deal with an error (May be a bug) of the Transporter position?

Genius
Genius

Hello,everyone 

I wanna use the "Transporter" as a Robot  to transfer the parts.

As is shown in the picture1: that what I want.I set the position of the Robot,and it shown the right position.

and it runs smoothly.

 

 

However,when I save it ,the position is wrong ,which is shown in the following picture2.

you can refer to it. the position is the same with the picture1. while the result is different. in my view,it goes back to the default setting. I dont konw why? How to dealt with it?

Looking forward to your directions,Thank you!

 

 

捕获.JPG

Picture1

 

 

 

01.JPG

 

picture2

 

 

 

 

 

1 REPLY

Re: how to deal with an error (May be a bug) of the Transporter position?

Siemens Phenom Siemens Phenom
Siemens Phenom

What you see in the picture is the position of the graphic in the MU called "Robot" relative to its owning object. As long as you do not change the graphic of the instance (which I do not recommend unless you need to do that), this is totally correct.

 

Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution