Cancel
Showing results for 
Search instead for 
Did you mean: 

how to draw the product out curve

Valued Contributor
Valued Contributor

as below figure1 ,I want to draw the curve of the product leave Drain;

I want to draw two curve, one is that  the drain exit number that in every hour(for example the first is 20,the second hour is 23,the third hour is 18,and so on ),and the effect  like picture 2

two is that I want to draw  the drain exit   accumulation curve ((for example the first is 20,the second hour is 20+23,the third hour is 20+23+ 18,and so on ),) thank you very much

捕获.PNG捕获.PNG

1 REPLY 1
Highlighted

Re: how to draw the product out curve

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

you can do this by plotting the attribute drain.StatThroughputPerHour for the hourly throughput and for the accumulated number of MUs you can plot the attribute drain.StatNumOut.

Kind regards,

Igor
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution