Cancel
Showing results for 
Search instead for 
Did you mean: 

is there a way to create a frame with the same characteristic of a transporter or an MU?

Builder
Builder

is there a way to assemble a frame on a transporter or create a frame with the same characteristic of a transporter that can get in a line and assume movement?

1 REPLY

Re: is there a way to create a frame with the same characteristic of a transporter or an MU?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Ricardo,

No, that's not possible.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.