Cancel
Showing results for 
Search instead for 
Did you mean: 

line backwards I have an urgent problem

Pioneer
Pioneer

捕获.PNGas below problem , when the mu move on line2-line6,I run the method "backwards" to make the mu move backwards,however the mu stop and donot move ,how can I solve it ,my plant version is 12.0

 

thank you  see the attachment 

6 REPLIES 6

Re: line backwards I have an urgent problem

Phenom
Phenom

if the lines (2..6) are > 2 x Container length,

 

then your method works.

Re: line backwards I have an urgent problem

Pioneer
Pioneer
@ simulator why the line 2>2 x Container length;
now the line is 6m and the container is the 5.8m this is the real data;
how can solve this? thank you very much

I test in version 13(create a new model) ,it works normal; but in 12 it has the problem ; how can solve thank you

Re: line backwards I have an urgent problem

Legend
Legend

Hi,

backward is not called. You can set a sensor on line6 to call this method.

 

sensor041218.jpgsensorasevent

regards
Nadin

Re: line backwards I have an urgent problem

Pioneer
Pioneer
@ nadin1223 no when the mu in line 2 or line3 or line4 or line5 I run the method "backwards" manually

Re: line backwards I have an urgent problem

Phenom
Phenom

@njIly

 

if you have to work with v12 you can subsitute

 

the lines2..6 through one 29 m (5 X 5.8m) line.

 

 

 

Re: line backwards I have an urgent problem

Legend
Legend

it could help to reverse the line

 

sensor041218.jpg