Cancel
Showing results for 
Search instead for 
Did you mean: 

moving entities from one transporter to another

Experimenter
Experimenter

Hi,
I created two tracks with one transporter on each. Track1 with transporter1 and track2 with transporter2.

Now I want to move entities at the end of track1 from transporter1 to transporter2 which waits at the start of track2. I did that with sensors. One sensor at the end of track1 and one at the start of track2.

I connected my methode with the sensor at the end of track2.

Then I wanted to move objects from transporter1 to transporter2 with "@.mu.move(transporter2);"

but it constantly tells me that transporter2 is a "unknown identifier".

I tried everything but I dont get any further.

Hopefully you have some tips Smiley Happy

thanks in advance

1 REPLY 1

Re: moving entities from one transporter to another

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
the error means, that no object exists with the name transporter2

open the transporter and have a look on the head of the dialog; the first transporter has the path
.MUs.transporter:1 the second .MUs.transporter:2

so you can write
@.mu.move(.MUs.transporter:2)

or indirectly
@.mu.move(track2.cont)


Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net