Cancel
Showing results for 
Search instead for 
Did you mean: 

mu transfer in a certain ratio

Pioneer
Pioneer

QUERY.JPG

how to achieve the case shown in image. MU A and MU B have been defined in class library and need to be transferred to main line in ratio 2:1. which is the easiest way to do so? I am still a software learner in an automobile OEM

5 REPLIES

Re: mu transfer in a certain ratio

Genius
Genius

Hello Aagosh,

 

Please find the model attached without programming.

 

 

Thanks & Best Regards,
Abhilash Sridhar
Mercedes Benz R&D India, Daimler AG

Re: mu transfer in a certain ratio

Pioneer
Pioneer

Dear Abhilash

 

Awesome, I am amazed simply using the assembly and dismantling block to maintain the ratio of mu a and b. that was awesome.

 

but another query how is ratio being maintained from source 1 and dummy 2 of and a and b is to c(entity in your model)?

 

suppose i had to put two c and 1 a and b like this- abccabccabcc

 

how to adjust ratio in this?

 

though i am bad at simtalk but I am open to learning

 

Also Sir another request from you, in another post I have mentioned how to display no. of each type of MUs on a line/buffer, etc. Can u suggest innovative way for that too.

Re: mu transfer in a certain ratio

Valued Contributor
Valued Contributor
You can use Flow Control object and set the Entry Strategy as "Cyclic Sequence". In the List Enter your MU A successor number two times and MU B successor number Once.

Re: mu transfer in a certain ratio

Valued Contributor
Valued Contributor
 

Re: mu transfer in a certain ratio

Pioneer
Pioneer

Thanks!..Works perfectly..