Cancel
Showing results for 
Search instead for 
Did you mean: 

multiple floor production line simulation model

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hello All,

I am looking for a simulation demo model for multiple floor production line to adapt customer request.

I would appreciate if you could share the idea for simulation method for displaying multiple floor factory model either 2D or 3D.

Thank you

 

1 REPLY 1

Re: multiple floor production line simulation model

Phenom
Phenom

Unfortunately the simulated multiple floor production lines

 

in the areas of Body & White,

 

I know of,  are all related to customer projects.

 

Therefore cannot be published at easily.

 

Self evident, the reason for using multiple floors  is

 

the need for space.

 

To link the production lines, on different levels,

 

usually lifts are installed to move the skids /carriers

 

up and down to the target level.

 

In 2D you can split the model into different levels/frames but

 

it doesn't have to be as the impact (through) floor change is

 

already defined by the elevators at the beginning and end of the

 

production line.