06-06-2015 03:14 AM
Respected Sir,
I have created a delivery table for my 4 job 7 machine flow shop problem. I need
to create pallets according to the size of the jobs entering into the system through delivery table. Because in my delivery table all jobs of size 5 is entering, but at the last interval, jobs of size 4 is entering. So pallet size of 5 is not suitable .I am enclosing the file here. Please help me.
06-08-2015 03:13 AM
Hello SIbi,
in your delivery table you can add the attribute XDim for the last enttries which only have a size of 4. For the attribute you can define the value 4 which will set the XDim of the created pallet to 4.
Regards
GG