Cancel
Showing results for 
Search instead for 
Did you mean: 

probability problem

Valued Contributor
Valued Contributor

as below figure,the v1  mean that  it will occur  with the  probability of  2% ,and t1 mean that the times that it happen that .      the v2  mean that  it will occur  with the  probability of  4% ,and t2 mean that the times that it happen that .     theoretically I think the times that v2   occur should  twice as big as v1, however they has a   big difference微信图片_20180828102042.png

I  donot  know why?

1 REPLY 1

Re: probability problem

Siemens Phenom Siemens Phenom
Siemens Phenom

to be accurate you have to:

  • use v:=z_uniform(1,0,100)
  • utilize the ExpMgr in order to get a valid result

to make the results more easy to understand I limited the number of parts created by the Source to 1000

 

spp in 14.1 (no 13.0 installation anymore)

 


Regards

Always consider using the AttributeExplorer!