Cancel
Showing results for 
Search instead for 
Did you mean: 

put two part one next the other on one line

Pioneer
Pioneer

 

Hi

I want to know if it is possible to put 2 MU . one next to the other on the same line  .it must look like this.

 

Please help me 

Thanks

 

13 REPLIES

Re: put two part one next the other on one line

Phenom
Phenom

you can do, if you e.g. place both Mus on a pallet which is on the line.

 

Unbenannt.png

Betreff: put two part one next the other on one line

Gears Phenom Gears Phenom
Gears Phenom

Hi Manu15,

I assume you want them to move along the line side-by-side. That's not possible, unless you use a container-MU that holds these two MU's. In this way, you can have them (look like they) travel side-by-side, but for the line-object, there is only 1 MU (the container-MU).

Best Regards,
Alex

___________________________________________________________
Alex Dilg, Consultant at SimPlan AG (www.SimPlan.de)
This post was good and/or helpful to you? Please provide some Kudos, thank you!

Betreff: put two part one next the other on one line

Pioneer
Pioneer

Hi

Thanks for this information.

I want that the robot take the first part on the line and  put on the container(in other line) and take the other part put next to the first ( I finally not choice to do it with the container). that is my code

But it don't work well because I have this message : Moving a part from a rotating station is not allowed.

Thanks

Betreff: put two part one next the other on one line

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

let the PickAndPlace do its job; this means: The first MU calls the pickAndPlace (e.g. connector). Use the exit control of the PickAndPlace to change the destination of the MU (stop the line, create the container, load into the container instead on the line).

The next MU will call the PickAndPlace again. Now use the exit control to load the part into the container (check if the line is stopped) and start the line.

 

 

see here an example for loading parts into a box using PickAndPlace:

https://www.bangsow.eu/detail_en.php?id=657

 

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Betreff: put two part one next the other on one line

Pioneer
Pioneer

My difficulties is to programm the robot to take a part and put next to the other on the same container.

it don't work like I want. The robot put one part on one container and if I stop line the robot is blocked because it don't arrive to put it

Betreff: put two part one next the other on one line

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
can you post your model?
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Betreff: put two part one next the other on one line

Pioneer
Pioneer
I can't because it is confidential. sorry.
The quick programm.I want to do is to take a part on line after the machine then put it on other line with pick and place.
The contraint is that the part must move side by side on the same line (it is not possible on line only I use container)
When the container is create on line , Pick and place take one part on the previous line put on the container the next line which have container must wait until the pick and place take another part and put next to the first on the same container.
After the line restart and transfer container to another line.
I don't know if you understand well what I want to do?
Please can you help me?
Thanks

Betreff: put two part one next the other on one line

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
it is difficult without a model. So please, extract this part from your model and post it.
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Betreff: put two part one next the other on one line

Pioneer
Pioneer

Capture is the programm in my robot(Robot2)

and Capture 3 is the programme on my first line  (LinePlaqueuse)where the part arrive after machine

The line(LineR1) which have container don't have any programm