Cancel
Showing results for 
Search instead for 
Did you mean: 

remote method setting transferstation status: working

Hi everybody,

 

 

My question, is it possible anyhow to set up a method with the ability to change the status of the transferstation to "working" by passing  a defined sensor on any conveyer even when the transferstation is empty.

 

It is just necessary for the time statistics.

 

 

greets.

1 REPLY

Re: remote method setting transferstation status: working

Siemens Legend Siemens Legend
Siemens Legend

By creating an MU on a  material flow object, it is always at the end of the process, i.e. it does not start at the beginning of the process time defined in the object. 

So you have to create the MU first, then "move" it to the object to start with the process time. You can create on another object, or on the same:

MUs.Entity.create(SingleProc)

SingleProc.cont.move(SingleProc)