Cancel
Showing results for 
Search instead for 
Did you mean: 

restarting the simulation and keeping the status information

Pioneer
Pioneer

Hello, I have maybe unusual request.

 

I want to know if there is a posibility on saving the status information of the whole simulation model when I press restart.

So when I press start again the simulation doesnt go from init state, but it goes from the state I restarted.

Any idea?

 

Thanks and regards 

6 REPLIES

Re: restarting the simulation and keeping the status information

Phenom
Phenom

you can save the simulation model at a required point

to then restore (reload) and run the model from the saved point again.

Re: restarting the simulation and keeping the status information

Pioneer
Pioneer

Can I do this with automatic with method? Beacuase I would need to do that many times.

Re: restarting the simulation and keeping the status information

Phenom
Phenom

look here:

 

Unbenannt.PNG

Re: restarting the simulation and keeping the status information

Pioneer
Pioneer

Hey there, 

 

there is something wrong with the picture - I just see a small triangle.

 

 

Re: restarting the simulation and keeping the status information

Siemens Phenom Siemens Phenom
Siemens Phenom

To keep the models MUs at reset and to (re)start from this status the next run you just need to remove the checkmark "Delete MUs on reset" on the Settings-tab of the EventController.


Regards

Always consider using the AttributeExplorer!

Re: restarting the simulation and keeping the status information

Phenom
Phenom

@HugoZupan 

 

as the posted screen shot is popping up and disappearing

 

again ,

 

have a look at the method "saveModel" in the help file.