Cancel
Showing results for 
Search instead for 
Did you mean: 

setup Time

Creator
Creator


Hallo Everyone,

 

I have problem in Modelling of Setup time. i have for each Part two Times Setup . the First one is befor the Starting of the Process and the Second is after finishing of the Process. how could I model them in the Same Station and how to make deffirent time of each of them.

 

Best Regard

 

Ali

 

7 REPLIES 7

Re: setup Time

Phenom
Phenom

Hi,

 

You can use the Recovery time for this case. 

Recovery time starts : When processing is finished.

 

2019-08-12 13_01_26-.png

Re: setup Time

Creator
Creator

Hi,

 

thank you for your fast Replay Smiley Happy

 

the Problem, that Both Setup Processes should be done by Worker. in Import there is no place to call worker to do this process and the Setup of the next Part will start during the Setup.

Re: setup Time

Phenom
Phenom

If you don't have a lot of variants, you can merge this with the setup of the next part and use the setup matrix to define the setup times.

 

=> For example, Setup between PartA and PartB will be (setup2 of PartA + setup1 of partB ) and this will be carried out always by the same worker.

 

 

 

Another(complex) way can be to call the setup importer in the exit control of the station.(Only if part on the previous station is different from the current part)

 

 

Re: setup Time

Creator
Creator

Another easy solution can be to add Loading Time at the Workplace itself. 

2_setups_before_after.JPG

Regards

Bhaiya

Re: setup Time

Phenom
Phenom

Hi @Alabboud 

 

You can control your system with methods, take a look at the model attached (PlantSim v15).

 

setupManual.PNGSetting-up the machine manually

Best Regards,
Paulo Araujo

Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: setup Time

Creator
Creator

Thank you very Much for your Example. it was very Helpful Smiley Happy

Re: setup Time

Creator
Creator

Hi,
thank you for your Replying me and your Answer. that will be wonderful, if the worker will Transport the Part from station to Another. in My Case the Part will be transported by overhead Crane.

 

 

best Regards


@Bhaiya wrote:

Another easy solution can be to add Loading Time at the Workplace itself. 

2_setups_before_after.JPG

Regards

Bhaiya



@Bhaiya wrote:

Another easy solution can be to add Loading Time at the Workplace itself. 

2_setups_before_after.JPG

Regards

Bhaiya