Cancel
Showing results for 
Search instead for 
Did you mean: 

somebody help me? can't save the PS object elements back to TC

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

 

if i open the ps from the TC, i can load every object like resources, part ,that's look good!

1.png

 

but if i created some object in PS,and update to TC, then error happend

2.png

find some erro message as below:

2016-06-28_18-29-16.png

 what i need to do?

Teamcenter9.1

Tecnomatix_10.1

Tecnomatix_10.1_TC_Alignment-16-x64

 

4 REPLIES

Re: somebody help me? can't save the PS object elements back to TC

Siemens Phenom Siemens Phenom
Siemens Phenom

This is the Plant Simulation Forum, not the Process Simulate Forum.

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: somebody help me? can't save the PS object elements back to TC

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter
where is the Process Simulate Forum.?

Re: somebody help me? can't save the PS object elements back to TC

Siemens Phenom Siemens Phenom
Siemens Phenom

It's the 'Tecnomatix Robotics Forum'.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: somebody help me? can't save the PS object elements back to TC

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter
thank you!
i have submited a new topic in this Forum