Cancel
Showing results for 
Search instead for 
Did you mean: 

source create mu

Valued Contributor
Valued Contributor

in my model,I want to create mu per some rule, namely everytimes create ten mus, and   I need create five times(manely fifty mus  in all), and the  interval between every times per "uniform",how can i do it

1 REPLY 1

Betreff: source create mu

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello fox,

 

assume you want to create the MUs on a object which I call station.

Create a methode with the following code:

var part: object := .MUS.Part.create(Station)

partsCreated += 1     // a global variable counting the number of parts created

// determine the waiting time as auniform distribution between 60and 120 seconds, using random stream 9

var waitingTime : time := z_uniform(9, 60, 120)

self.methcall(waitingTime)     // call the method again after the waiting time has gone

 

 

Hope this helps

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution