Cancel
Showing results for 
Search instead for 
Did you mean: 

start plantsimulation in hidden mode

Legend
Legend

Hello,

 

I want to start a plantsimulation instance without any interface. Just like experiment manager does.

 

In the documentation I see Start Options /hibeBBL but it "Hide Plant Simulation after starting it"

 

Is there a way to start plant simulation in hidden mode and not start and after hide it ? 

 

Regards,

 

rpinon

6 REPLIES

Re: start plantsimulation in hidden mode

Phenom
Phenom

You can start Plant Simulation through the COM interface and

 

switch on/off visibility ( s. setVisible)

 

Default is non visible

Re: start plantsimulation in hidden mode

Legend
Legend

Hello,

 

If you are using a shortcut to launch the application, right click to open Properties...

In the Shortcut tab, change option from dropdown menu from 'Normal Window' to 'Minimized'

 

 

Unbenannt111.png

Re: start plantsimulation in hidden mode

Legend
Legend

I want to start plant simulation with commande line. 

 

If I understand simulator I need to develop an other program to start plantsimulation in hidden mode ?? Smiley Frustrated

 

Regards,

 

rpinon

Re: start plantsimulation in hidden mode

Phenom
Phenom

It's not just running PS on command line level.

 

COM is an Interface to PS including the features  to fully hide & communicate with PS.

 

Yes, you need some (available) language to call Plant Simulation through COM Interface

 

This could be vbScript available on command line level

 

or EXCELvba.

 

I have to check if I have some vba script to run the COM-Interface  on comand line level.

 

 

Re: start plantsimulation in hidden mode

Legend
Legend

So, there is no built-in solution to do that ? (for me COM interface in not a solution)

Re: start plantsimulation in hidden mode

Phenom
Phenom

Just in case you change your opinion about built in solutions.

 

Here's the vbs code to start Plant Simulation hidden.

 

set oSim = CreateObject("Tecnomatix.PlantSimulation.RemoteControl.14.1")
osim.setVisible(false)

wrap the code in a *.vbs  file and run the file from the command line level with cscript *.vbs