Cancel
Showing results for 
Search instead for 
Did you mean: 

student license 80 objects

Experimenter
Experimenter

Hello,

 

I just got the student license and wanted to start make my model. But then I saw, that I am already over 80 objects. Is that the object library?

If yes, how should I make a simulation model with this student license? I can delete some of the objects but that is a little strange solution to the problem.

 

Are there other ways except from buying a full license?

 

Best regards

Nik

2 REPLIES 2

Re: student license 80 objects

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi Nick,

 

add a method in the frame with the following content:

is
do
 print numOfLimitedObjects;
end;

 

This shows how many (limited) objects already in your model.

Select File - Manage Class Library. Uncheck all elements, you don't need; especially uncheck (if possible) all elements in the tab Libraries.

 

Best regards

 

Steffen

 

 

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: student license 80 objects

Experimenter
Experimenter

Hi Steffen,

 

Thanks!

The problem were some of the libraries..I activated some of the tools. Not sure if I will need them so I deactivated them for now and got down with the objects. Now I can start building my model.

 

Best regards

Nik