Cancel
Showing results for 
Search instead for 
Did you mean: 

the object XPOS and Ypos

Pioneer
Pioneer

as below shown, In 3D model ,the object "S1"  its xpos and ypos as below shown   ,and I open s1 3d properties  its  position  as below picture too,  I  want to know the distinguish between “Xpos/ ypos” and " x/y position"  thank you very much

 TIM图片20180522121330.png

5 REPLIES

Betreff: the object XPOS and Ypos

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello njily,

 

the XPOS and YPOS are defined in pixel coordinates of the 2D frame. 

<obj>._3D.Position gives the position of the object in meter or any other unit according to your settings.

 

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Betreff: the object XPOS and Ypos

Pioneer
Pioneer
hello GG:
can they have conversion between ”XPOS 、 YPOS “ and position

Betreff: the object XPOS and Ypos

Siemens Phenom Siemens Phenom
Siemens Phenom

I would advise to use <obj>.Coordinate3D instead of <obj>._3D.Position

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Betreff: the object XPOS and Ypos

Pioneer
Pioneer
dear MichaelJoos、GG

I donot understand well about <obj>.Coordinate3D and <obj>._3D.Position and “XPOS and Ypos”;can you explain more about them, and can you tell me how to have conversion between them; thank you very much
Highlighted

Betreff: the object XPOS and Ypos

Phenom
Phenom

Before literally posting, what is written in the help file,

 

I suggest , that you have a look in the same.