Cancel
Showing results for 
Search instead for 
Did you mean: 

two lines production

Pioneer
Pioneer

Hi,

 

Question:

1. One Container from Line2 can only be attached to one Part in the "Assembly" machine. The model is blocked, but I don't how to solve this problem.

 

2. The capacity of each buffer is 9. Normally, two buffers are full of MUs. For example, if one ContainerA appears in Line2, a PartA from BufferA goes to the "Assembly" machine. Further, if there are less PartA in the buffer, compared with the number of PartB in BufferB, Line1 is called to make one PartA. I am not sure which code I can use. I am a beginner of Plant Simulation. Does anyone know any code please?

Thanks for your help. I use Plant Simulation V12.0.

 

Kind Regards

Loki

8 REPLIES 8

Betreff: two lines production

Valued Contributor
Valued Contributor
 

Re: two lines production

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
For your first questions the answer lies with your Assembly Station. The way an Assembly station works without an assembly table is it requires a product from each predecessor. In your current model there are no products in BufferB, as such it cannot receive a part from this predecessor.

For the second section, you are currently making products whenever you create a Container at your Source. This Source gets blocked as soon as you create the 2nd Container, because the Assembly is still waiting for / processing parts. Why don't you just make 9 of each parts at the start of your Simulation at the Line1_SP?

Re: two lines production

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

if you want to assembly one PartA on ContainerA and one PartB on containerB you need to change the assembly list (MU types) of the assembly station depend on the name of the container you create.

You can extend your method runPartType (and you should run it as a entrance control before actions of the assembly station):

 

is
do
	
	local assList:table[string,integer];
	assList.create;
	If @.Name = "ContainerA" then
		.MUs.PartA.Create (Line1_SP);
		assList[1,1]:="PartA";
		assList[2,1]:=1;
		assembly.assemblyList:=assList;
		
	else
		.MUs.PartB.Create (Line1_SP);
		assList[1,1]:="PartB";
		assList[2,1]:=1;
		assembly.assemblyList:=assList;
		
	end;
	
end;

To fill your buffers the first time you could use a method with the name init. This is called at  the start of the experiment:

 

 

do
	while bufferA.full=false loop
		.MUs.PartA.create(bufferA);
	end;
	
	while bufferB.full=false loop
		.MUs.PartB.create(bufferB);
	end;
	
	
end;
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: two lines production

Pioneer
Pioneer

Hi Sebastiaan,

 

Thansk for your reply. I add a MU type table in the Assembly machine. It works now, thank you.

 

For the second question. My idea is that Line1 produces 9 of each parts at the start of the work every day. Those parts wait in the buffer until a container comes in Line2. If it's ContainerB, PartB goes to "Assembly". After a working period, there might be less PartA in BufferA than the number in BufferB. Then, Line1 automatically produces PartA. It's difficult that I know how to make it work. I hope I make it clear.

 

Cheers

Betreff: two lines production

Pioneer
Pioneer

Hello Simpulse,

 

Many thanks for your help, but the model is still blocked.

 

 

Kind Regards

Loki

Re: two lines production

Pioneer
Pioneer

Hello.

 

sorry to bother you, I have done what you taught in the last message, but the model is blocked at some points.

I have no idea how to fix this kind of problem. Can you help me?

 

Thank you

Re: two lines production

Valued Contributor
Valued Contributor
Check the spelling of "Assemblylist". There is a misspelling. Smiley Happy

Re: two lines production

Pioneer
Pioneer

Yeah, you are right. God, finally I finish it. Thank you, and thank everyone.