Cancel
Showing results for 
Search instead for 
Did you mean: 

unload assembly station

Creator
Creator

I have some troubles with unloading an assembly station. I have a set of 3 assembly stations in parallel fed by one singleproc (see figure). What I would like is that any entity (not a container) from pre-successor 2 which is entering the assembly station with a atribute unload = true will force to unload the content of all the 3 assembly stations even if they are not full. 

 

I tried to do it with the following programming on the entrance of the assembly stations, but it doesn't works since it will only check the atributes of the containers:

 

if @.unload = true then
@.move;
assembly.cont.move;
assembly1.cont.move;
assembly2.cont.move;
end;

 

anyone an idea how? 

 

question.PNG    

1 REPLY

Re: unload assembly station

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
you could try this as the exitcontrol of the SingleProc

if @.unload = true then
@.move;
wait(1);
assembly.cont.move;
assembly1.cont.move;
assembly2.cont.move;
else
@.move;
end;
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net