Cancel
Showing results for 
Search instead for 
Did you mean: 

usability of machines : M1 , M2, M4

Pioneer
Pioneer

Hi,

My main goal in this model is more usability of machines-Working  : M1 ,M2, M4

m1m2m4.jpg

 

I trying to improve little usability for M1 and M2 and I use this Method in M1 -(Controld-Exit)


is
do
if M2.occupied and M2.operational and
B1.full then
@.move(Buffer);
else
@.move(B1);
end;
end;

 

What else can I do with methods to improve  usability, maybe in BufferB2 (Controls-Exit) for M4? or is this enough , or I need to put a few SingleProc to imrpove usability : M1, M2 , M4 ?

23092014.jpg

 

 

Best regards,

Andreas Domuz

2 REPLIES

Re: usability of machines : M1 , M2, M4

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hello Andreas,

 

look in the statistic. You have a high processing time in M3, so you block M2 and M1 and M4 shows a lot of waiting time.

 

In such cases you have to look on the process, if it is possible e.g. to move parts of the processing from M3 to M2, M1/ M4 or increase the capacity in M3 (e.g. 2 machines).

 

The other bottleneck is M5 and M6...

 

 

 

 

Best regards

 

Steffen

 

 

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: usability of machines : M1 , M2, M4

Pioneer
Pioneer

Thank you so much