Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

using a formula for arrivals

Valued Contributor
Valued Contributor

Dear community members, 

i need to create a source with the following distribution for arrival times:

6.99 * BETA(0.362, 3.1)

If I select formula and I type the above formula, the result is disappointing: it creates too many entities. Do I make any mistake?

 

Also, is it possible to run multiple simulations automatically and have a summary file with average, maximum and minimum values?

 

Thank you

3 REPLIES 3

Re: using a formula for arrivals

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

the formula looks good,

should work in this way as interval in the source:

6.99 * z_BETA(?.randomSeed,0.362, 3.1)

 

I hope you know, the values are seconds, with the Beta-distribution you get a mean interval of round about 0.7  seconds.

 

 

"is it possible to run multiple simulations automatically and have a summary file with average, maximum and minimum values?"

 

yes, try the experiment manager

 

 

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: using a formula for arrivals

Valued Contributor
Valued Contributor

Thank you for your reply.

Do you know also how can I transform the values in minutes instead of seconds?

Re: using a formula for arrivals

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

just muliply it with 60

 

6.99 * z_BETA(?.randomSeed,0.362, 3.1)*60

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net