Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

v14 connector from class library

Creator
Creator

We are migrating to v14.0.1 and noticed that the Connector is only accessible via the Toolbox. Drag and Connect from the Class Library /MaterialFlow Folder is not possible. Is there a preferences selection that enables the connector via the class library?

2 REPLIES

Re: v14 connector from class library

Siemens Phenom Siemens Phenom
Siemens Phenom
Hi! Try to hold Ctrl key when dragging connector from class library.
Regards, Vladimir.

Re: v14 connector from class library

Creator
Creator

Thx, this is the solution works.