Cancel
Showing results for 
Search instead for 
Did you mean: 

v14 connector from class library

Creator
Creator

We are migrating to v14.0.1 and noticed that the Connector is only accessible via the Toolbox. Drag and Connect from the Class Library /MaterialFlow Folder is not possible. Is there a preferences selection that enables the connector via the class library?

2 REPLIES 2

Re: v14 connector from class library

Siemens Phenom Siemens Phenom
Siemens Phenom
Hi! Try to hold Ctrl key when dragging connector from class library.
Regards, Vladimir.

Re: v14 connector from class library

Creator
Creator

Thx, this is the solution works.