Cancel
Showing results for 
Search instead for 
Did you mean: 

visual glitch in 14.0.1

Legend
Legend

Hi everyone,

 

Since I update to 14.0.1 (before 13.2) I have a lot of glitch with my 2D stack structure.
image.png

One container has (fictively) a different conveying direction than the other in stack. When I click on the frame "groupe", all glitch disapeare. Like that :

image.png 

I attach the model. So you can repeat the bug.

[reset => run in fast mode => stop/toogle Mus animation]

 

Best regards,

 

rpinon

2 REPLIES 2

Re: visual glitch in 14.0.1

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi rpinon,

 

unfortunately there is a bug when drawing loaded MUs on rotated frames for the first time after fast forward mode.

We will fix the bug in the next maintenance packs.

 

Kind regards

Karola

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: visual glitch in 14.0.1

Legend
Legend

Hi, Thanks for reply

 

I am looking forward to see that,

 

Regards,

 

rpinon