Cancel
Showing results for 
Search instead for 
Did you mean: 

worker move freely teleportation

Legend
Legend

Hi,

 

I have a problem with the worker.goTo method.

 

When I say to 2 workers to go to the same place [goto(place1,false)], the 2nd one push the 1st one out of the place.

So its location is workpool but visualy on "place1".

After that I say to worker1 goto(place2,false). Worker1 is teleported far away from "place1" and go to "place2"

 

See attach a model witch show the bug.

 

The transport task lasts longer. it is a problem for several simulation because I use it a lot...

 

Regards,

 

rpinon

 

3 REPLIES 3

Re: worker move freely teleportation

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi rpinon,

 

There is a bug when a "pushed aside" worker was sent with goto. This will be fixed in the next maintenance pack.

 

Regards,

Karola

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: worker move freely teleportation

Legend
Legend
Hi,

Thanks,

When will the next maintenance pack be realesed ?

Regards,
rpinon

Re: worker move freely teleportation

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

It is planned that the next maintenance pack will be released at 07.07.2018.

If you have a maintenance contract and badly need a bugfix, you can create a PR at GTAC and then get a hotfix for the problem.

 

Regards,

Karola

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.