Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

worker not carrying part properly

I have a situation where the worker have to carry part from two machines. A model attached shows the exact situation. 

The worker has capacity 1. I want the worker to empty the machine 1 first and then only start carrying from the machine 2. For example first part from machine 1 the again the 2 part from the machine 1, now the 3 part from machine 2 and 4 part from machine 2.

but the problem is that the worker carry first part from machine 1 but goes to machine 2 after that and then come back to machine 1 and then again to machine 2. 

can someone help me how to control the worker in this case ?

 

attached is small model of what i am trying to do!!

2 REPLIES 2

Re: worker not carrying part properly

Phenom
Phenom
if you give machine1 a higher priority than machine 2

then it will work for this case

Re: worker not carrying part properly

Thanks Phenom!! that will work!!