Cancel
Showing results for 
Search instead for 
Did you mean: 

(worker) problem in the new version 14.0.2

Experimenter
Experimenter

Hi,

i’ve got a problem with the new version 14.0.2 of Plant Simulation.

If i run my simulation of production processes (with a lot of machines, MUs, methods, workerPools etc.) in the new version, i have less output (statNumOut) compared to a run in the old version (14.0.1), but there was no change in the production processes, it’s exactly the same. Especially the StatServicesWorkingPortion of the workers is less than before (in the old version).

Does anyone have similar problems with the new version?

Thanks in advance!

1 REPLY 1

Re: (worker) problem in the new version 14.0.2

Siemens Phenom Siemens Phenom
Siemens Phenom

Dear Experimenter,

You are right, a significant change in the simulation results should not occur from one version to another.

Can you give us the 14.0.1 model?

Regards

Peter