Cancel
Showing results for 
Search instead for 
Did you mean: 

worker showing wrong data in statistics??

Hello community,

 

I have a weird situation with the worker.

When i dont provide any failure to the worker, the statistics shows the correct data. but when i put the failure in failure profiles, the end statistics are wrong. I am not able to understand the reason. I have put the picture for reference

Can anybody guess what is going wrong here '?

 

Thanks in advance!!!!

9 REPLIES 9

Re: worker showing wrong data in statistics??

Siemens Phenom Siemens Phenom
Siemens Phenom
Thanks for your attention! It´s hard to say something just based on screenshots ... (so one reason could be just not not to have refreshed the dialog) ... anyway, in case you assume to have revealed a bug, please be so kind to use File/Help/Log an Incident with Technical Support and/or File/Help/Upload a File to Technical Support. In case your license is not under maintenance and you want to stay in the forum the model should be attached.

Regards

Always consider using the AttributeExplorer!

Re: worker showing wrong data in statistics??

Gears Phenom Gears Phenom
Gears Phenom

I would find it interesting to see the model, because I cannot reproduce it; so hopefully you can upload it here Smiley Happy

And the statistics really seem odd (if the worker has walked these distances, how come he's been waiting 99% of the time? And why is the exporter statistic failed for 5%, but not the worker?)

Here's an example screenshot in Plant 14

grafik.png

Regards,
Alex

___________________________________________________________
Alex Dilg, Consultant at SimPlan AG (www.SimPlan.de)
This post was good and/or helpful to you? Please provide some Kudos, thank you!

Re: worker showing wrong data in statistics??

Hello Mr. AlexD,

 

That is exactly the problem. I am not able to find the reason. 

It might happen that I am doing something wrong but again I created another small model to simulate the same thing and I am again observing the same problem. 

attached is the model.

It would be great If you could let me know whats happening.

Danke!!

Re: worker showing wrong data in statistics??

Siemens Phenom Siemens Phenom
Siemens Phenom
I can´t see any problem there! Where did you modify the failure behavior? I guess you did it at the instance of the worker, which is not the right way, because MUs will be created at init again. You should create a dedicated class for your resource and parameterize this one.

Regards

Always consider using the AttributeExplorer!

Re: worker showing wrong data in statistics??

I have modified the failure behaviour in the class itself. If you look in my model attached above. The worker failure is given in the class of the resources. But still it is not showing the right value.

Re: worker showing wrong data in statistics??

Gears Phenom Gears Phenom
Gears Phenom

When I run your model, the statistics look fine to me:

grafik.png

Do you have other results? I'm using Plant 13.0.6

Alex

Edit: Oops, I just saw that @Eventdebugger has posted the same screenshot, I assumed it was from a separate model.

___________________________________________________________
Alex Dilg, Consultant at SimPlan AG (www.SimPlan.de)
This post was good and/or helpful to you? Please provide some Kudos, thank you!

Re: worker showing wrong data in statistics??

Yes!! I am getting different result when i run it in my model(see screenshots).

I am using version 13.0.0

 

It might be a bug. Is there any way to check it ?

Re: worker showing wrong data in statistics??

Gears Phenom Gears Phenom
Gears Phenom

It is a bug and it has already been fixed. Please update your software to the latest patch version, this will solve your problem.

___________________________________________________________
Alex Dilg, Consultant at SimPlan AG (www.SimPlan.de)
This post was good and/or helpful to you? Please provide some Kudos, thank you!
Highlighted

Re: worker showing wrong data in statistics??

Hi Alex_D,

thank you for confirming it. I will update it to the latest patch asap and hopefully it works fine