Cancel
Showing results for 
Search instead for 
Did you mean: 

worker

Builder
Builder

i have 8 workers working on a single proc.each worker when finishes the work ,it comes to a buffer ,carry the part and work at the station.similarly when other worker is free he comes to the buffer ,carry the part and work there.Problem is how i can write a method on the exit cntrl of buffer so that which ever worker is free he comes to the buffer on its own and  carry the part...i have tried a lot of things but not getting satisfactiry results...i just want to model a situation where whihcever worker is free he comes to the store ,takes the part and so on..

Need Help!!!!

4 REPLIES 4

Re: worker

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi k_parashar,

 

You can use a buffer with exit strategy "Carry part away" to get the worker carry the part to a station and work on it. But I think you need to sketch the system a bit more clearly. If there is a fixed combination of storage space and work station, then you can use separate buffers.

 

Regards,

Gert Nomden


Gert Nomden
Senior Consultant | Tecnomatix Product Manager
cardsplmsolutions.com

Re: worker

Builder
Builder

i am using carry part away but the problem is in the mutarget,i can only feed one destination there.but the destination changes each time.i am not able to write a method for MU target where mu target changes to the workplaces where the worker finished the job.

Re: worker

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

So, as soon as the worker has finished a job, there is a new one waiting? You can use an exit control at the workstation to push a new MU from the storagebuffer. For the buffer you then should implement an exit control (front-triggered) that first sets the destination, then applies the move command. Once you attempt to move the MU, the service request is made. I did not test it now, but I am 98% sure that this would work.


Gert Nomden
Senior Consultant | Tecnomatix Product Manager
cardsplmsolutions.com

Re: worker

Hi

 

I had a similar problem

 

And I did something like this...

 

    -- What is the type on the carier, that need to be carried away
    PartName := @.cont.name;

 

-- Set the destination according to the object type and where it is supose to go

-- Look in a table to find the needed destination

@.Destination := str_to_obj(to_str(DestTable["Line Address", PartName]));