Cancel
Showing results for 
Search instead for 
Did you mean: 

writeXMLFile and format

Legend
Legend

Hello everyone,

 

I have a question regarding writeXMLFile. Is there any way to also save the format of the table with this method like with writeFile when writing .obj files?

 

If not, is there a possibility to add this functionality?

 

Best regards

4 REPLIES

Re: writeXMLFile and format

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello verbalins,

At the moment only the data type of the column is written to the XML file.

Of course it is possible to enhance this, but at the moment we have no plans.

Is there anything specific you'd like to have?

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: writeXMLFile and format

Legend
Legend
Hello Ralf,

In the best of worlds I would like it to have the same information as the obj-file. But the most difficult has been to preserve the format of nested sub-tables.

I would have no problem with the obj-file if two saved obj-files from the same table had the same SHA-sum. Now when two obj-files from the same table are compared they do not have the same SHA-sum.

Re: writeXMLFile and format

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello verbalins,

In the upcoming version 13.1 we will change the obj file format so that two files do not differ when saved multiple times.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: writeXMLFile and format

Legend
Legend
Thank you Ralf!