Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Presentation: Introduction to SimTalk 2.0

Community Manager Community Manager
Community Manager

Introduction to SimTalk 2.0       

Presenter: Michael Joos, Siemens Industry Software GmbH, Germany 

We moderately enhanced SimTalk in order to increase user-friendliness. Michael Joos gives an overview of the syntax changes and the new features, comparing the old and new syntax. This includes variable and parameter declarations, loops, default arguments and more. He also shows how to automatically convert SimTalk 1.0 Methods into the new SimTalk 2.0 syntax. When you load a model, which you saved in a previous version of Plant Simulation, it will run without changes.

SimTalk 1.0 Methods and SimTalk 2.0 Methods can be used in the same model in parallel.

The ribbon button Method > Tools > New Syntax independently sets for each Method if the source code has to be entered in SimTalk 1.0 or SimTalk 2.0 syntax

24_Joos_Simtalk_2_0.png

Michael JoosMichael Joos

 

                   

Highlighted

Presentation: Introduction to SimTalk 2.0

Community Manager Community Manager
Community Manager

Introduction to SimTalk 2.0       

Presenter: Michael Joos, Siemens Industry Software GmbH, Germany 

We moderately enhanced SimTalk in order to increase user-friendliness. Michael Joos gives an overview of the syntax changes and the new features, comparing the old and new syntax. This includes variable and parameter declarations, loops, default arguments and more. He also shows how to automatically convert SimTalk 1.0 Methods into the new SimTalk 2.0 syntax. When you load a model, which you saved in a previous version of Plant Simulation, it will run without changes.

SimTalk 1.0 Methods and SimTalk 2.0 Methods can be used in the same model in parallel.

The ribbon button Method > Tools > New Syntax independently sets for each Method if the source code has to be entered in SimTalk 1.0 or SimTalk 2.0 syntax

24_Joos_Simtalk_2_0.png

Michael JoosMichael Joos