Cancel
Showing results for 
Search instead for 
Did you mean: 

FastTrack and Subversive updates released

Dreamer
Dreamer
A new version of FastTrack, the free tracker plugin for Eclipse is now available. The update is directed at those who are currently using Eclipse 3.1. This release is mainly to provide compatibility with a new update release of Subversive, a free Subversion client for Eclipse, which is distributed together with, and used by FastTrack. FastTrack 1.0.5 (which includes Subversive 1.0.5) may be downloaded here: http://powerversion.com/downloads/fasttrack/1.0.5/ Important note:
Subversive 1.0.5 is the last release in the 1.0.x stream, which is frozen from that version. We will continue development on the 1.1.x stream, which will be migrated to the eclipse.org site, and also will work on the new version targeted at the upcoming Eclipse 3.3. You can get Subversive 1.0.5 alone at the following URLs: Update site:
http://www.polarion.org/projects/subversive/download/update-site/ Archived Update Site and Source Code downloads:
http://www.polarion.org/index.php?page=download&project=subversive