Showing results for 
Search instead for 
Do you mean 

Log-Rotation for Apache

by Dreamer on ‎07-14-2008 12:29 AM

The following statement will enable log rotation for Apache. The command is specified for installation in a Windows system. Please check paths for you own installation. CustomLog "|C:/Polarion3.1.1/bundled/apache_2.0.59/bin/rotatelogs.exe C:/Polarion3.1.1/data/logs/apache/access.log 60" common Log rotation works by a pipe to the rotatelogs.exe, which itself can be configured to rotate logs by time or by size. Try rotatelogs -? to get help. The given statement is suitable for the access log file, which receive most of the log output. Look for further log configuration in httpd.conf and adopt them appropriately to rotate all Apache log files. Best Wishes Matthias