Cancel
Showing results for 
Search instead for 
Did you mean: 

Morris Medical Monday: Polarion MedPack Traceability

Dreamer
Dreamer
Welcome back to Morris Medical Monday: a weekly series for medical device development companies (and companies who are related to such companies), providing some useful information about Polarion solutions and Polarion extensions. Today we will continue on the subject of Polarion's MedPack extension, and have a look into MedPack's Traceability.

Traceability

Along with reviews, providing traceability (see IEC 62304:3006->3.32) between deliverables (see IEC 62304:3006->3.6) is one of the main requirements of IEC 62304. By providing traceability it can be proved that decisions have been thoroughly reflected and possible consequences have been considered. Therefore, it is one of the most important factors for quality and patient and user safety, which is the focus of IEC 62304.

Traceability Requirements of IEC 62304:2006

The picture below shows the traceability requirements for the deliverables of IEC 62304:2006 with dashed lines. The labels describe the type of link and the clause of the standard requiring the links (in brackets). MedPack represents most of these deliverables with Work Items, some with dedicated wiki pages. Traceability

How MedPack handles traceability

Traceability is provided by Polarions' standard link roles. However, special link roles according to the diagram above are defined for MedPack's work item types. The table below shows these link roles. MedPack Link Roles
traceability meaning impact meaning Description
traces to leads to Used for decision traceability.
covers covered by Used for relations between documentation and development artifacts.
implements implemented by Used for relations between concepts and concrete deliverables implementing those.
part of decomposed into Used to describe relationships of architectural elements (SW System, SW Item, SW Unit and SOUP)
detected by detects Used for relations of qm measures and resulting error descriptions.
The provision of links is not enforced in any way, any work item can be created, modified and closed without any checks. This keeps MedPack flexible for any kind of development lifecycle model. However, checking and analysing the existences of links is a focus of the wiki pages in the Product Documentation Wiki For more information about Polarion's MedPack visit our Extension Portal using following link: http://extensions.polarion.com/extensions/31-polarion-alm-medpack-iec-62304. I hope you liked this article and you will visit our blog again when there is another Morris Medical Monday article.

Webinar Banner: Medical Device Innovator Adopts a full ALM Framework