Showing results for 
Search instead for 
Do you mean 

Morris Medical Monday: Work Item Types "SOUP"

by Dreamer on ‎01-05-2015 03:00 PM

Welcome back to the first Morris Medical Monday article of the new year. I hope you had a great holiday season. For anyone who is new to our blog, this a weekly series for medical device development companies (and companies who are related to such companies), providing some useful information about Polarion solutions and Polarion extensions. Today we will continue on the subject of Polarion's MedPack extension, and have a look into MedPack's SOUP Work Item.

Soup

Description

A description of a software component of unknown provenance (SOUP) used in the project, according to clause 3.29 of IEC 62304:2006. Any issue of this type must be linked to the software item that is implemented by the component.

Workflow Steps

The SOUP Work Item uses the standard Evaluation Workflow. EvaluationWorkflow_Overview

Traceability & Impact

A SOUP Work Item must be traceable to a Software Item Work Item and a Architectural Design Work Item and has an impact on an Integration Test Work Item and a Hazardous Situation Work Item. For more information on traceability and impacts, see the Traceability wiki page.

Attributes

Special hyperlink roles

A SOUP work item has special hyperlink roles to fulfill the requirements of IEC 62304. The following tables lists thos roles.
Hyperlink Role Description
Published anomaly list URL of an anomaly list for the used SOUP component
SOUP manufacturer URL of the manufacturer's homepage.
SOUP URL URL of additional information about the SOUP component.

Work Item Attributes

The following custom fields must be filled out before evaluation can be requested:
Attribute Name Type Description
SOUP title Text (as required by IEC 62304:2006->8.1.2a).
SOUP manufacturer Text (as required by IEC 62304:2006->8.1.2b).
SOUP designator Text (as required by IEC 62304:2006->8.1.3c).
System hardware and software requirement [B,C] Text Example: Processor type, storage type, system-software type,...(as required by IEC 62304:2006->5.3.3).
Functional and performance requirement [B,C] Text (as required by IEC 62304:2006->5.3.4).

Evaluation Attributes

The following custom fields must be filled out before evaluation can be finshed and the work item can be closed:
Attribute Name Type Description
Reviewer Text Person(s) to perform, performing or have performed a review.
Review summary Text Short summary of the review. Attachments should be used for additional information.
Last review date Date Hidden field automatically set when review has been finshed. Intended to be used for sorting and statistical analysis.

Evaluation Checklist

The following checklist must be filled out before evaluation can be finshed and the work item can be closed:
Checklist entry Description

Possible Resolutions

The following table shows the possible resolution values when the work item is closed:
Resolution Name Description
Ready For Use The SOUP element has been evaluated and can be used in the product.
Obsolete The SOUP element has become obsolete and is no longer needed.
Discarded The work item entry has been discarded. No further attention is needed.
For more information about Polarion's MedPack visit our Extension Portal using following link: http://extensions.polarion.com/extensions/31-polarion-alm-medpack-iec-62304. I hope you liked this article and you will visit our Blog again when there is another Morris Medical Monday article

Read how medical device company LifeWatch succeeds with Polarion: Polarion Customer Success Story: LifeWatch