Cancel
Showing results for 
Search instead for 
Did you mean: 

Morris Medical Monthly: How to use RiskPack (Part 2 of 4)

Dreamer
Dreamer
Welcome back to Morris Medical Monthly: a monthly series for medical device development companies (and companies who are related to such companies), providing some useful information about Polarion solutions and Polarion extensions. Today we will start on the subject of Polarion's RiskPack extension, and have a look how to use RiskPack.

Planning: Choose the right data model

Define the starting point for your risk management

Before you can start using the RiskPack for a live project, it is necessary to define a starting point for your risk management. If you described your product with functional requirements, they can be the starting point for your risk analysis. If you already know the architecture and the components of your device, they could be the starting point, too. "Starting point" means the type of information (i.e. the work item type) that is the beginning of the sequence of events that finally will lead to a harm. If you do a more general risk analysis, even the possible hazards can form the starting point, but they could also "only" be a part in the sequence of events. Figures 1 to 3 show three options for modeling sequences of events. The RiskPack Default Template uses the data model shown in figure 1.

figure1 Figure 1: Sequence of events starting with functional requirements (click for larger image)

figure2 Figure 2: Sequence of events starting with functional and physical interfaces (click for larger image)

figure3 Figure 3: Sequence of events starting with hazards (click for larger image)

Planning: Define process, team and risk policy

Document risk management process

Use the Risk Management Process wiki page to document your approach to risk management or refer to another document which contains a process description.

Document risk management team members

Use the Risk Management Team wiki page to document the risk management team for this project.

Ensure risk acceptance levels are appropriate

Define the risk acceptance levels according to your company. Use the Risk Acceptance Editor for this. At least two levels are required: A level for acceptable risks and a level for unacceptable risks. You can define as many level in between as suitable. It is common to have a third level called "ALARP", so this is predefined in the template.

Ensure proper categories for the severity of harm

Ensure that the categories for the severity of harm are suitable for your project. The predefined values are just an example. Adapt them to your needs.

Ensure proper categories for the probability of occurrence of a harm

Ensure that the categories for the probability of occurence of a harm are suitable for your project. The predefined values are just an example. Adapt them to your needs.

Define risk acceptability

Use the Risk Acceptance Editor to define acceptability for all severity/probability combinations.

Review Risk Policy

Use the Risk Policy wiki page to review your risk policy settings.   For more information about Polarion's RiskPack visit our Extension Portal using following link: http://extensions.polarion.com/extensions/184-polarion-alm-riskpack-iso-14971. I hope you liked this article and you will visit our Blog again when there is another Morris Medical Monthly article.
Medical device solutions by Polarion