Cancel
Showing results for 
Search instead for 
Did you mean: 

Polarion Meets the Bionic Man - "Must-see" Webinar

Dreamer
Dreamer
The "Six-million Dollar Man" of the old American TV series is not yet reality, but something like that reality is getting closer all the time, especially at Polarion customer Rex Bionics Ltd. Rex Bionics research teamA phenomenally innovative and advanced robotics technology company, Rex Bionics' scientists and engineers are developing a solution enabling wheelchair users (and others with a mobility impairment) to stand and walk, allowing them to be independently upright and mobile.Their solution is a robotic exoskeleton called Rex. This Thursday, October 24, Toby Martin, Software Test Lead at REX Bionics will present a free live webinar, in which he'll talk about the implementation and development of processes used for software testing team within the highly regulated medical device environment, using an integrated approach to software and device risk management as per ISO 14971, while complying with IEC 60601 and IEC 62304 medical device regulations. Rex Bionics has a truly amazing story. If you attend no other Polarion webinar this year, don't miss this one!
MISSED THE LIVE WEBINAR? NO PROBLEM. IT'S NOW AVAILABLE ONLINE:
Polarion webinar banner - Medical Innovator Adopts Full ALM Solution