Cancel
Showing results for 
Search instead for 
Did you mean: 

Change process step from code

Experimenter
Experimenter

Hi,

is there a way to change the process step programmatically?

Say I wanted to go to the next process step once a Boolean property becomes True. Is there anything like rootpart.ProcessSteps.GoToStep(ID)?

I only found information to read the current process step.

 

Thank you,

Adrian

3 REPLIES

Re: Change process step from code

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Adrian,

 

Here are a couple of snippets of code that should work for you.

 

This one will find the next process step:

 

Public Function ProcessStepNext() As String

        Dim nextProcessStep As ProcessStep = Nothing

        Dim currentIndex As Integer = -1

 

        For i As Integer = 1 To rootpart.ProcessSteps.Count

            Dim oProcessStep As ProcessStep = CType(rootpart.ProcessSteps.Item(i), ProcessStep)

            If oProcessStep.Name = rootpart.currentProcessStep.split("\")(1) Then

                currentIndex = i

                Exit For

            End If

        Next

 

        If currentIndex > -1 Then

            For i As Int32 = currentIndex + 1 To rootpart.ProcessSteps.Count

                Dim oProcessStep As ProcessStep = CType(rootpart.ProcessSteps.Item(i), ProcessStep)

                If oProcessStep.Status <> ProcessStepStatus.Disabled AndAlso _

                 oProcessStep.Status <> ProcessStepStatus.Hidden Then

                    nextProcessStep = CType(rootpart.ProcessSteps.Item(i), ProcessStep)

                    Exit For

                End If

            Next

        End If

 

        Return nextProcessStep.name

    End Function

 

This one will let you pick the Process Step to navigate to:

 

SetProcessStep("YourProcessStepName", YourPartFamily)

 

  'Function that finds a specified process step and returns the object

    Private Sub SetProcessStep(ByVal sproc As String, ByRef epart As Part)

 

        'selected process step

        Dim sProcessStep As ProcessStep = Nothing

 

        'loop through all procesteps, find the process step passed by sproc

 

        For i As Integer = 1 To RootPart.ProcessSteps.Count

            Dim oProcessStep As ProcessStep = CType(RootPart.ProcessSteps.Item(i), ProcessStep)

            If oProcessStep.Name.Contains(sproc) Then

                sProcessStep = oProcessStep

                Exit For

            End If

        Next

 

        g_RsEngineer.SelectProcessStep(sProcessStep, epart, -1, 0)

 

    End Sub

 

Best Regards,

Trent

Re: Change process step from code

Experimenter
Experimenter

Thank you, Trent - that looks exactly like what I was looking for.

Re: Change process step from code

Valued Contributor
Valued Contributor

A note about this code - because of the way Rulestream tears down the custom UI (using enumeration), if you were to change the process step within a WhenChanged formula, you will likely see an error message because he tear down happens in the middle of the enumeration. To avoid this, use the action button (not the regular button) and tie it to a method in Custom.vb and run this code from there (unless this already fixed in later versions).

 

Dharmesh