Cancel
Showing results for 
Search instead for 
Did you mean: 

Comparing 2 or more LineItems

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi All,

did any one of you need a comparison of two or more Line Items?

And if yes what had to be compared? Inputs, Dependent Properties?

Did you solve this via Component Database?

 

regards

Thomas

4 REPLIES 4

Re: Comparing 2 or more LineItems

Valued Contributor
Valued Contributor

I'm not sure that this can help but you can compare XML files for each line item.

Re: Comparing 2 or more LineItems

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi,

this might probably be a good alternative, since OutputTable is typically filled in on Release. And not inbetween or before releases.

 

regards

Thomas

Re: Comparing 2 or more LineItems

Siemens Genius Siemens Genius
Siemens Genius

Hi Thomas,

 

did you try to query through the project database with an dynamic query?

 

BR

Christian

Re: Comparing 2 or more LineItems

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

I tested it right away and I think this would be the approach i will follow.