Cancel
Showing results for 
Search instead for 
Did you mean: 

Grid doesn't refresh properly

Experimenter
Experimenter

I have a grid in my custom UI design which is connected to a subpart. The quantity of this subpart depents on a property value from the parent part family. When the quantity is changed the bounded grid doesn't refresh properly. It refrehses itself correctly only after the user is activating the it (by clicking in the grid). Attached is a video which shows it. Is there a way to solve this?

 

Many thanks!

1 REPLY 1

Re: Grid doesn't refresh properly

Experimenter
Experimenter

I found the solution, just put the following line under the "When changed" tap of the subpart collection

g_RsEngineer.RefreshModelViews(0)

Important: Don't forget to set the AutoSetRsEngineer on "True" otherwise it will give an no instance error.

 

 

Setting.PNG