Cancel
Showing results for 
Search instead for 
Did you mean: 

How to retrieve uploaded filename when using File Import Spec

Experimenter
Experimenter

I'm trying to upload a file into the Rulestream application using the File Import custom UI control and the File Import Spec.  The file import is working to the point of getting the file copied into the working folder, but instead of having the file name I expect (filname.ext), it is getting a prefix added to it (3770_161_filname.ext).  I assume I should be able to retrieve the uploaded file name from the File Import Spec, but how?

2 REPLIES 2

Re: How to retrieve uploaded filename when using File Import Spec

Valued Contributor
Valued Contributor

Isn't prefix related with project ID and Lineitem ID?

If so, knowing the rule you can forecast the name.

Or you can retrieve the file just after file import by looking for most recent file or specyfing seach filter to find a file where name contains something.Both using Directory.GetFiles() method

Adam Liszkiewicz
Configuratori Polska

Re: How to retrieve uploaded filename when using File Import Spec

Valued Contributor
Valued Contributor

Hi

As I encountered the same issue with using File Import spec in ThinClient I asked this question to Siemens guys and recieved an answer.

Imported file name is stored in spec attributes.

So following code allows to retrieve exact name of uploaded file:

If fileSpec IsNot Nothing AndAlso fileSpec.Attributes.Count >= 2 Then
importedFileName = fileSpec.Attributes(2).Value
End If
Where fileSpec object is your FileImport spec

 

Adam Liszkiewicz
Configuratori Polska