Cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to lock a project line item so a user can’t delete it?

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Question from a customer.

 

Gene

 

Gene Libardi
Principal Solutions Architect
Engineering Intent Corporation
www.EngineeringIntent.com


3 REPLIES 3

Re: Is it possible to lock a project line item so a user can’t delete it?

Genius
Genius

Not sure but if you will prohibit for specific users editting the databases on the database management system side possibly they will not be able to modify properties and remove lineitems as well.

Seems we had a problem looking like that.

Re: Is it possible to lock a project line item so a user can’t delete it?

Valued Contributor
Valued Contributor

You may try with setting readonly permission for application for such user (but I don't know if that will work).

Other way is setting lineitem as Shareable but this would can be changed by the user and then he/she can delete.

 

Last thing that comes to my mind is a nasty (in terms of performance) database approach.

To create trigger on update of LineItems table and if Deleted column value is set to 1 and user performing operation should not be able to delete, disregard it. But this trigger will slow any activity on lineitems (as it will be fired on every update).

A bit better (in terms of performance) is having a task/service that will check and undelete lineitems deleted by users without permissions. This will also increase database traffic but if done i.e. 1-2 times per day should not be noticeable.

Adam Liszkiewicz
Configuratori Polska

Re: Is it possible to lock a project line item so a user can’t delete it?

Valued Contributor
Valued Contributor
No line item or project is ever deleted. There is a column in the database that is set to 1 (true) when it is deleted. So if a line item is ever deleted it can be recovered by resetting the value to 0.